Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Method and Description |
---|---|
RunItemsBuilder |
DefineRunBuilder.createRunItemsBuilder()
Creates a RunItems used to create list item for DefineRun
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") . |
RunItemsBuilder |
RunItemsBuilderList.findItem(int index)
Returns the object at the input index.
|
RunItemsBuilder[] |
RunItemsBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
RunItemsBuilderList.append(RunItemsBuilder object)
Appends an object to the list
License requirements: None. |
void |
RunItemsBuilderList.append(RunItemsBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
RunItemsBuilderList.erase(RunItemsBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
RunItemsBuilderList.erase(RunItemsBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
RunItemsBuilderList.findIndex(RunItemsBuilder obj)
Finds the index where the input object appears.
|
void |
RunItemsBuilderList.insert(int location,
RunItemsBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
RunItemsBuilderList.setContents(RunItemsBuilder[] objects)
Sets the contents of the entire list.
|
void |
RunItemsBuilderList.swap(RunItemsBuilder object1,
RunItemsBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.