Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static RunItem.Type |
RunItem.Type.FROM
A "From" item type.
|
static RunItem.Type |
RunItem.Type.MEMBER
A "Member" item type
|
static RunItem.Type |
RunItem.Type.TO
A "To" item type
|
Modifier and Type | Method and Description |
---|---|
RunItem.Type |
RunItem.itemType()
Returns the Run Item type such as "From", "To", or "Member" item.
|
static RunItem.Type |
RunItem.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RunItem.Type |
RunItem.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RunItem.Type[] |
RunItem.Type.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AssignPathBuilder.addToScopedObjectSet(NXObject object,
RunItem.Type runItemType)
Add the given object to the scoped object set
License requirements: routing_base ("Routing Basic") . |
RunItem |
RouteManager.createRunItem(String referenceID,
RunItem.Type itemType,
CharacteristicList attributes)
Creates a new
RunItem . |
void |
RunItem.setItemType(RunItem.Type itemType)
Sets the Run Item type such as "From", "To", or "Member" item.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.