Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static Run.Status |
Run.Status.BROKEN
Run is broken.
|
static Run.Status |
Run.Status.INCOMPLETE
Run is incomplete.
|
static Run.Status |
Run.Status.VALID
Run is valid.
|
Modifier and Type | Method and Description |
---|---|
Run.Status |
Run.edit(String runId,
String runType,
NXObject[] from,
NXObject[] to,
NXObject[] member)
Edits an existing run with new items.
|
Run.Status |
Run.getRunStatus()
Ask the status of run
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") . |
static Run.Status |
Run.Status.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Run.Status |
Run.Status.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Run.Status[] |
Run.Status.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.