Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
nxopen.routing.electrical |
Provides classes and interfaces for Routing Electrical.
|
Modifier and Type | Interface and Description |
---|---|
interface |
AssemblyDefinition
Represents a collection of
SingleDevice objects that are used in an assembled product. |
interface |
ConnectivityDefinition
The base class for various connection objects.
|
interface |
DeviceRelationship
Represents a relationship between
SingleDevice objects. |
interface |
InterfaceTerminalBase
The
InterfaceTerminalBase corresponds to an abstract class for
a prototype Port . |
interface |
InterfaceTerminalRelationshipBase
|
interface |
InterfaceTerminalRelationshipShadow
Represents an assembly shadow of
InterfaceTerminalRelationshipBase . |
interface |
InterfaceTerminalShadow
Represents the defining data for a physical
Port . |
interface |
ItemDefinition
ItemDefinition object corresponds to DDID in AP212 and to a piece
part or routing stock in NX. |
interface |
LogicalConnection
Represents a connection between mutiple From and To
LogicalTerminal . |
interface |
LogicalTerminal
Assembly instance of a
InterfaceTerminalBase . |
interface |
ObjectRelationship
Represents a relationship between Routing objects.
|
interface |
PartDefinitionBase
The abstract class
PartDefinitionBase contains
information defining a logical part. |
interface |
PartDefinitionShadow
PartDefinitionShadow contains the defining data for a
logical part, such as an connector. |
interface |
RouteObject
The Top level routing data model object.
|
interface |
SingleDevice
The Routing SingleDevice corresponds to an abstract instance of
ItemDefinition . |
interface |
StockDefinition
Represents Routing StockDefinition object
Creator not available in KF. |
interface |
StockDevice
The Routing StockDevice corresponds to a generic stock instance
of
SingleDevice . |
Modifier and Type | Method and Description |
---|---|
RootObject |
RouteManager.findRoutingObject(RouteManager.SearchCriteria searchCriteria)
Returns the Routing object, if any, that matches the given search criteria.
|
RootObject[] |
RouteManager.getSelectedObjectsInNavigators()
Returns all of the objects selected in the Component and Connection Navigators.
|
Modifier and Type | Method and Description |
---|---|
void |
RouteManager.selectObjectInNavigator(RootObject objectToSelect)
Highlights the given object in the Component or Connection Navigator.
|
void |
RouteManager.selectObjectsInNavigator(RootObject[] objectsToSelect)
Highlights the given objects in the Component or Connection Navigator.
|
Modifier and Type | Interface and Description |
---|---|
interface |
CableConnection
Connection used by a
CableDevice . |
interface |
CableDefinition
Holds the collection of wires in a
CableDevice . |
interface |
CableDevice
Corresponds to a cable instance of an
ElectricalStockDevice . |
interface |
CableStockDefinition
Describes a cable's stock.
|
interface |
Connection
The electrical usage of a
LogicalConnection , restricted to
one From and one To terminal. |
interface |
ConnectorDevice
The Electrical ConnectorDevice corresponds to a connector instance of
SingleDevice . |
interface |
ElectricalDeviceRelationship
Represents a relationship between Routing Electrical devices.
|
interface |
ElectricalPartDefinitionShadow
Represents
ElectricalPartDefinitionShadow object Creator not available in KF. |
interface |
ElectricalStockDefinition
Represents
ElectricalStockDefinition object Creator not available in KF. |
interface |
ElectricalStockDevice
The Electrical Stock Device is a non instantiable superclass to classify
all electrical stock-based single devices.
|
interface |
HarnessDefinition
Represents a
HarnessDefinition Creator not available in KF. |
interface |
HarnessDevice
The Electrical HarnessDevice corresponds to a harness instance of the
SingleDevice . |
interface |
JumperConnection
A jumper connection connects ports on the same connector.
|
interface |
NonPathConnection
Describes a connection that does not have a path
A pathless connection represents the abilitiy for objects to be connected even though there is not an explicit path between them. |
interface |
PathConnection
Describes a connection that has a path
From and To terminals are not coincident and need a path definition to be routable. |
interface |
ShieldDefinition
Represents Routing Electrical ShieldDefinition object
Creator not available in KF. |
interface |
ShieldDevice
The Electrical ShieldDevice corresponds to a shield instance of
ElectricalStockDevice . |
interface |
ShieldStockDefinition
Represents Routing Electrical ShieldStockDefinition object
Creator not available in KF. |
interface |
SystemDefinition
Represents a
SystemDefinition Creator not available in KF. |
interface |
SystemDevice
The Electrical SystemDevice corresponds to a system instance of the
SingleDevice . |
interface |
WireDevice
The Electrical WireDevice corresponds to a wire instance of
ElectricalStockDevice . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.