Package | Description |
---|---|
nxopen.mechanicalrouting |
Provides classes and interfaces for Mechanical Routing.
|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Method and Description |
---|---|
void |
PartPlacementBuilder.setClassificationObjectIdentifierOfCompatibilityPart(ReuseLibrary.PartType ccType,
String classificationObjectId,
Port portOne,
Port portTwo)
Sets the identifier of the classification object associated with the compatibility part to post place
License requirements: routing_base ("Routing Basic") . |
Modifier and Type | Field and Description |
---|---|
static ReuseLibrary.PartType |
ReuseLibrary.PartType.BOLT
Bolt Post Placement Type
|
static ReuseLibrary.PartType |
ReuseLibrary.PartType.GASKET
Gasket Post Placement Type
|
static ReuseLibrary.PartType |
ReuseLibrary.PartType.NUT
Nut Post Placement Type
|
static ReuseLibrary.PartType |
ReuseLibrary.PartType.RINGJOINT
Ring Joint Post Placement Type
|
static ReuseLibrary.PartType |
ReuseLibrary.PartType.STUD
Stud Post Placement Type
|
static ReuseLibrary.PartType |
ReuseLibrary.PartType.UNKNOWN
Unknown Type
|
static ReuseLibrary.PartType |
ReuseLibrary.PartType.WASHER
Washer Post Placement Type
|
static ReuseLibrary.PartType |
ReuseLibrary.PartType.WELDRING
Weld Ring Post Placement Type
|
Modifier and Type | Method and Description |
---|---|
static ReuseLibrary.PartType |
ReuseLibrary.PartType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ReuseLibrary.PartType |
ReuseLibrary.PartType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ReuseLibrary.PartType[] |
ReuseLibrary.PartType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RouteManager.createConnectionPostPlacementUdo(ReuseLibrary.PartType udoType,
int numberOfItems,
ReuseLibrary.ReportInBom reportInBOM,
CharacteristicList udoCharx,
PortConnection[] connectionsToLink)
Creates a user defined object (UDO) linked to one or two connections.
|
void |
ReuseLibrary.specificationsDefinePostPlacementRules(String specName,
ReuseLibrary.PartType partType,
String startingIdentifier,
String[] searchAttributes)
Defines Post Placement rules.
|
ReuseLibrary.SpecificationsGetPostPlacementRulesData |
ReuseLibrary.specificationsGetPostPlacementRules(String specName,
ReuseLibrary.PartType partType)
Gets post placement rules.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.