Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static PortConnectionCollection.PortsStatus |
PortConnectionCollection.PortsStatus.CAN_CONNECT
The Ports can be connected
using Port Connection object.
|
static PortConnectionCollection.PortsStatus |
PortConnectionCollection.PortsStatus.CANNOT_CONNECT
The Ports cannot be connected
using Port Connection object.
|
Modifier and Type | Method and Description |
---|---|
PortConnectionCollection.PortsStatus |
PortConnectionCollection.canPortsConnect(Port port1,
Port port2)
Determines if the two ports can be connected using a
PortConnection object. |
static PortConnectionCollection.PortsStatus |
PortConnectionCollection.PortsStatus.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PortConnectionCollection.PortsStatus |
PortConnectionCollection.PortsStatus.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PortConnectionCollection.PortsStatus[] |
PortConnectionCollection.PortsStatus.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.