Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
PortConnection |
RouteManager.ModelConnectionPostPlacementGasketData.connectionone
One of the new gasket flange connections
|
PortConnection |
RouteManager.ModelConnectionPostPlacementGasketBetweenFlangesData.connectionone
One of the new gasket flange connections
|
PortConnection |
RouteManager.ModelConnectionPostPlacementGasketData.connectiontwo
The other new gasket flange connection
|
PortConnection |
RouteManager.ModelConnectionPostPlacementGasketBetweenFlangesData.connectiontwo
The other new gasket flange connection
|
Modifier and Type | Method and Description |
---|---|
PortConnection |
Port.connect()
Finds another
Port to connect this port to. |
PortConnection |
PortConnectionCollection.createPortConnection(Port port1,
Port port2)
Creates a
PortConnection object. |
PortConnection |
PortConnectionCollection.getConnectionFromPort(Port port)
Returns the
PortConnection the given part participates in, if any. |
PortConnection |
Port.getPortConnection()
If port is connected to another port, returns the Port Connection that links them.
|
Modifier and Type | Method and Description |
---|---|
void |
RouteManager.createConnectionPostPlacementUdo(ReuseLibrary.PartType udoType,
int numberOfItems,
ReuseLibrary.ReportInBom reportInBOM,
CharacteristicList udoCharx,
PortConnection[] connectionsToLink)
Creates a user defined object (UDO) linked to one or two connections.
|
RouteManager.ModelConnectionPostPlacementGasketData |
RouteManager.modelConnectionPostPlacementGasket(Component placedPart,
PortConnection connection,
ReuseLibrary.ReportInBom reportInBOM,
CharacteristicList gasketCharx)
Places a gasket part based on the gasketCharx
CharacteristicList . |
RouteManager.ModelConnectionPostPlacementGasketBetweenFlangesData |
RouteManager.modelConnectionPostPlacementGasketBetweenFlanges(Component placedPart,
PortConnection connection,
ReuseLibrary.ReportInBom reportInBOM,
CharacteristicList gasketCharx)
Places a gasket part based on the gasketCharx
CharacteristicList . |
void |
RouteManager.modelConnectionPostPlacementWeldGap(Component placedPart,
PortConnection connection,
double gapValue)
Places a weld gap by adding a weld gap characteristic to one of the part occurrences connected.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.