Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static Port.FlowDirectionType |
Port.FlowDirectionType.FLOW_NONE |
static Port.FlowDirectionType |
Port.FlowDirectionType.ROUTE_FLOW_EITHER |
static Port.FlowDirectionType |
Port.FlowDirectionType.ROUTE_FLOW_IN |
static Port.FlowDirectionType |
Port.FlowDirectionType.ROUTE_FLOW_OUT |
Modifier and Type | Method and Description |
---|---|
Port.FlowDirectionType |
Port.getFlowDirection()
Get the value of flow direction of
Port
License requirements: routing_base ("Routing Basic") Created in NX5.0.0 |
static Port.FlowDirectionType |
Port.FlowDirectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Port.FlowDirectionType |
Port.FlowDirectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Port.FlowDirectionType[] |
Port.FlowDirectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Port.setFlowDirection(Port.FlowDirectionType flowDirection)
Set the flow direction value of
Port
License requirements: routing_base ("Routing Basic") Created in NX5.0.0 |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.