Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static Port.CreateRotationVector |
Port.CreateRotationVector.NO
Do not create the rotation vector on the port created from a coordinate system.
|
static Port.CreateRotationVector |
Port.CreateRotationVector.YES
Create the rotation vector on the port created from a coordinate system.
|
Modifier and Type | Method and Description |
---|---|
static Port.CreateRotationVector |
Port.CreateRotationVector.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Port.CreateRotationVector |
Port.CreateRotationVector.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Port.CreateRotationVector[] |
Port.CreateRotationVector.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
FixturePort |
FixturePortCollection.createFromCsys(CartesianCoordinateSystem csys,
Port.CreateRotationVector createRotationVector)
Creates a fixture port based on an existing Cartesian Coordinate System.
|
FittingPort |
FittingPortCollection.createFromCsys(CartesianCoordinateSystem csys,
Port.CreateRotationVector createRotationVector)
Creates a fitting port based on an existing Cartesian Coordinate System.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.