Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static OverstockBuilder.WrapType |
OverstockBuilder.WrapType.OVERLAP_SPIRAL
Overlap Spiral
|
static OverstockBuilder.WrapType |
OverstockBuilder.WrapType.SPOT
Spot
|
static OverstockBuilder.WrapType |
OverstockBuilder.WrapType.STRIPED_SPIRAL
Striped Spiral
|
static OverstockBuilder.WrapType |
OverstockBuilder.WrapType.UNKNOWN |
Modifier and Type | Method and Description |
---|---|
static OverstockBuilder.WrapType |
OverstockBuilder.WrapType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OverstockBuilder.WrapType |
OverstockBuilder.WrapType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OverstockBuilder.WrapType[] |
OverstockBuilder.WrapType.values()
Returns an array that contains the values for this enum.
|
OverstockBuilder.WrapType |
OverstockBuilder.wrapMethod()
Returns the
OverstockBuilder.WrapType for Wrapped overstock. |
Modifier and Type | Method and Description |
---|---|
void |
OverstockBuilder.setWrapMethod(OverstockBuilder.WrapType wrapMethod)
License requirements: routing_advanced ("Routing Advanced") OR routing_harness ("Routing Harness") OR routing_cabling ("Routing Cabling") OR routing_pipetube ("Routing Piping and Tubing") OR routing_hvac ("Routing HVAC") OR routing_platform ("Routing Platform") OR routing_pid ("Routing PID") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.