Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static OverstockBuilder.PointType |
OverstockBuilder.PointType.END
End
|
static OverstockBuilder.PointType |
OverstockBuilder.PointType.MIDDLE
Middle
|
static OverstockBuilder.PointType |
OverstockBuilder.PointType.START
Start
|
Modifier and Type | Method and Description |
---|---|
OverstockBuilder.PointType |
OverstockBuilder.pointDefines()
Returns the defining point location which can be any of
OverstockBuilder.PointType
for OverstockBuilder.ApplicationType.POINT_AND_LENGTH method. |
static OverstockBuilder.PointType |
OverstockBuilder.PointType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OverstockBuilder.PointType |
OverstockBuilder.PointType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OverstockBuilder.PointType[] |
OverstockBuilder.PointType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OverstockBuilder.setPointDefines(OverstockBuilder.PointType pointDefines)
License requirements: routing_advanced ("Routing Advanced") OR routing_harness ("Routing Harness") OR routing_cabling ("Routing Cabling") OR routing_pipetube ("Routing Piping and Tubing") OR routing_hvac ("Routing HVAC") OR routing_platform ("Routing Platform") OR routing_pid ("Routing PID") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.