Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Method and Description |
---|---|
InterfaceTerminalShadow[] |
PartDefinitionShadow.getInterfaceTerminalShadows()
Returns the
PartDefinitionShadow 's associated
InterfaceTerminalShadow s. |
InterfaceTerminalShadow[] |
InterfaceTerminalRelationshipBase.getRelatedInterfaceTerminals()
Gets the list of
Port s in the InterfaceTerminalRelationshipBase
object with a relationship of related. |
InterfaceTerminalShadow |
InterfaceTerminalRelationshipBase.getRelatingInterfaceTerminal()
Gets the
Port in the InterfaceTerminalRelationshipBase
with a relationship of relating. |
InterfaceTerminalShadow |
LogicalTerminal.interfaceTerminalShadow()
Returns the
InterfaceTerminalShadow corresponding to Port in piece part. |
Modifier and Type | Method and Description |
---|---|
void |
InterfaceTerminalRelationshipBase.addRelatedInterfaceTerminal(InterfaceTerminalShadow relatedInterfaceTerminal)
Adds a
Port to the InterfaceTerminalRelationshipBase object
with a relationship of related. |
void |
InterfaceTerminalRelationshipBase.removeRelatedInterfaceTerminal(InterfaceTerminalShadow relatedInterfaceTerminal)
Removes a related
Port from the list of related terminals in the
InterfaceTerminalRelationshipBase object. |
void |
InterfaceTerminalRelationshipBase.replaceRelatedInterfaceTerminals(InterfaceTerminalShadow[] relatedInterfaceTerminals)
Replaces the existing related
Port s in the InterfaceTerminalRelationshipBase
object with input ones. |
void |
InterfaceTerminalRelationshipBase.setRelatingInterfaceTerminal(InterfaceTerminalShadow relatingInterfaceTerminal)
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.