Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static IntegrateRunsBuilder.Enum |
IntegrateRunsBuilder.Enum.FIRST_RUN |
static IntegrateRunsBuilder.Enum |
IntegrateRunsBuilder.Enum.SECOND_RUN |
Modifier and Type | Method and Description |
---|---|
IntegrateRunsBuilder.Enum |
IntegrateRunsBuilder.runAttributes()
Returns the run attributes
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") . |
static IntegrateRunsBuilder.Enum |
IntegrateRunsBuilder.Enum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static IntegrateRunsBuilder.Enum |
IntegrateRunsBuilder.Enum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static IntegrateRunsBuilder.Enum[] |
IntegrateRunsBuilder.Enum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
IntegrateRunsBuilder.setRunAttributes(IntegrateRunsBuilder.Enum runAttributes)
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.