Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Method and Description |
---|---|
Point |
PointCollection.createPoint(IRoutePosition routePosition,
Xform xform,
SmartObject.UpdateOption updateOption)
Creates a
Point at the given IRoutePosition . |
Modifier and Type | Interface and Description |
---|---|
interface |
Anchor
A Routing Anchor defines a position in a Qualified Routing component part.
|
interface |
ControlPoint
Routing Control Points define a position in space, and are used to determine connections
from segments to segments, and segments to ports.
|
interface |
ExtractPort
Routing ExtractPort object is an extract of Port class
To create an instance of this class use PortCollection.createExtractPort(nxopen.routing.Port) Created in NX4.0.0 |
interface |
FittingPort
Represents a Routing Fitting Port Object
FittingPort . |
interface |
FixturePort
FixturePort objects are objects that
segments are routed through when creating a routing path. |
interface |
IAxisPort
Interface class for all routing objects that specify a direction .
|
interface |
MultiPort
Represents a
MultiPort . |
interface |
Port
Routing Port Object is a parent class for FixturePort, ExtractPort, FittingPort,
Multiport, StockPort and TerminalPort
Creator not available in KF. |
interface |
ProxyPort
A
ProxyPort is a port that represents a connector in
another design zone, but not present in this design zone. |
interface |
StockOffsetPort
StockOffsetPort class handles the relationship
between a component part's port occurrence and the dumb offset port in
the work part. |
interface |
StockPort
|
interface |
TerminalPort
A
TerminalPort models the pins on an electrical
connector. |
Modifier and Type | Method and Description |
---|---|
ControlPointCollection.CreateControlPointData |
ControlPointCollection.createControlPoint(IRoutePosition startObject,
Vector3d offset,
ControlPointCollection.CheckExisting checkExisting)
Creates a dumb
ControlPoint object. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.