Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Interface and Description |
---|---|
interface |
OffsetPath
The Routing OffsetPath object is the set of information needed to define an offset route.
|
interface |
Path
The Routing Path object is the set of ordered continuous segments.
|
interface |
Wire
The Routing Wire object is the set of information needed to define
a ROUTE_wire.
|
Modifier and Type | Method and Description |
---|---|
IPath |
OffsetPath.getMasterPath()
The master path object for this offset object.
|
IPath[] |
OffsetPath.getOffsetPaths()
Returns the list of all of the offset paths for a master path
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") . |
Modifier and Type | Method and Description |
---|---|
void |
OffsetPath.setMasterPath(IPath masterPath)
The master path object for this offset object.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.