Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static HealMethod |
HealMethod.DIRECT |
HealMethod |
HealPath.AllData.healMethod |
static HealMethod |
HealMethod.INTERSECT |
static HealMethod |
HealMethod.MAX |
static HealMethod |
HealMethod.XYZ |
static HealMethod |
HealMethod.XZY |
static HealMethod |
HealMethod.YXZ |
static HealMethod |
HealMethod.YZX |
static HealMethod |
HealMethod.ZXY |
static HealMethod |
HealMethod.ZYX |
Modifier and Type | Method and Description |
---|---|
HealMethod |
HealPath.getHealMethod()
Get heal method.
|
static HealMethod |
HealMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HealMethod |
HealMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HealMethod[] |
HealMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HealPath.setAllData(Point3d startPoint,
Point3d endPoint,
Vector3d startVector,
Vector3d endVector,
double startParm,
double endParm,
double startExtension,
double endExtension,
boolean reverseStart,
boolean reverseEnd,
HealMethod healMethod,
SplineOptions splineOptions)
Set all the data associated with the heal path creation.
|
void |
HealPath.setHealMethod(HealMethod healMethod)
Set heal method.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.