Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static DivisionsBuilder.SplitDirectionType |
DivisionsBuilder.SplitDirectionType.SPLIT_HORIZONTALLY
Creates a horizontal split
|
static DivisionsBuilder.SplitDirectionType |
DivisionsBuilder.SplitDirectionType.SPLIT_VERTICALLY
Creates a vertical split
|
Modifier and Type | Method and Description |
---|---|
DivisionsBuilder.SplitDirectionType |
DivisionsBuilder.splitDirection()
Returns the direction of split, either vertical or horizontal
License requirements: routing_hvac ("Routing HVAC") . |
static DivisionsBuilder.SplitDirectionType |
DivisionsBuilder.SplitDirectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DivisionsBuilder.SplitDirectionType |
DivisionsBuilder.SplitDirectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DivisionsBuilder.SplitDirectionType[] |
DivisionsBuilder.SplitDirectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DivisionsBuilder.setSplitDirection(DivisionsBuilder.SplitDirectionType splitDirection)
License requirements: routing_hvac ("Routing HVAC") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.