Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static DeviceRelationship.RelationType |
DeviceRelationship.RelationType.ASSOCIATED_EQUIPMENT
the related single devices are attached to the relating single device
|
Modifier and Type | Method and Description |
---|---|
DeviceRelationship.RelationType |
DeviceRelationship.relationshipType()
Returns the type of the relationship.
|
static DeviceRelationship.RelationType |
DeviceRelationship.RelationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DeviceRelationship.RelationType |
DeviceRelationship.RelationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DeviceRelationship.RelationType[] |
DeviceRelationship.RelationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DeviceRelationship.setRelationshipType(DeviceRelationship.RelationType relationshipType)
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.