Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static CustomManager.NavigatorType |
CustomManager.NavigatorType.COMPONENT
The objects were selected in the component navigator.
|
static CustomManager.NavigatorType |
CustomManager.NavigatorType.CONNECTION
The objects were selected in the connection navigator.
|
Modifier and Type | Method and Description |
---|---|
static CustomManager.NavigatorType |
CustomManager.NavigatorType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CustomManager.NavigatorType |
CustomManager.NavigatorType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CustomManager.NavigatorType[] |
CustomManager.NavigatorType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CustomManager.NavigatorObjectSelectedPlugin.navigatorObjectSelectedPlugin(CustomManager.NavigatorType navigatorType,
CustomManager.SelectionType selectionType,
NXObject[] selectedObjects)
This defines the prototype Routing calls whenever an object on the Component or
Connection Navigator is selected or deselected.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.