Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.ASSIGN_STOCK
Called after the Assign Stock command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.ATTR_DISCREPANCY
Called after the Place Part and Replace Part commands.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.ATTRIBUTE_COPY_REPLACE_PART
Called after the Replace Part command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.BROKEN_CONNECTION
Called after a port-to-port connection is broken.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.CHOOSE_PART
Called after the Choose Part command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.COPY_PATH
Called after the Copy Path command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.COUNT
The number of callback reasons.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.CREATE_CONNECTION
Called after the Create Connection command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.CREATE_PORT_CONNECTION
Called after the creating a connection between two ports.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.CREATE_RUN
Called after the Create Run command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.DELETE_PATH
Called after the Delete Path command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.EDIT_CONNECTION
Called after the Edit Connection command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.EDIT_REPLACE_PART
Unused.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.MOVE_PART
Called after the Move Part command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.MOVE_PATH
Called after the Move Path command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.OFFSET_PATH
Called after the Offset Path command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.PLACE_PART
Called after the Place Part command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.REMOVE_PART
Called after the Remove Part command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.REPLACE_PART
Called after the Replace Part command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.REPLACE_STOCK
Called after the Replace Stock command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.RUN_PRE_DELETE
Called before deleting a run.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.TRANSFORM_PATH
Called after the Transform Path command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.UNASSIGN_STOCK
Called after the Remove Stock command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.UNKNOWN
Used only for validation.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.WIRE_COMP_AUTO
Called after the AutoAssign command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.WIRE_COMP_MANUAL
Called after the Manual Assign command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.WIRE_COMP_PROXY
Called after the Assign Proxy command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.WIRE_ROUTE_AUTO
Called after the AutoRoute command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.WIRE_ROUTE_MANUAL
Called after the Manual Route command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.WIRE_TERMINALS
Called after the Model Terminals command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.WIRE_UNCOMP
Called after the Unassign Component command.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.WIRE_UNROUTE
Called after the Unroute command.
|
Modifier and Type | Method and Description |
---|---|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CustomManager.CallbackReason |
CustomManager.CallbackReason.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CustomManager.CallbackReason[] |
CustomManager.CallbackReason.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
int |
CustomManager.addCallback(CustomManager.CallbackReason reason,
CustomManager.Callback callbackMethod)
Adds the callback with the given reason.
|
int[] |
CustomManager.getCallbacksRegisteredForReason(CustomManager.CallbackReason reason)
Returns the callbacks, if any, registered for the given reason.
|
void |
CustomManager.removeAllCallbacksForReason(CustomManager.CallbackReason reason)
Removes all the callbacks registered for a particular reason.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.