Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static CornerTypeBuilder.BendOptions |
CornerTypeBuilder.BendOptions.BEND_RADIUS_TABLE
Deprecated.
Bend table method creates bend from specified bend table
|
static CornerTypeBuilder.BendOptions |
CornerTypeBuilder.BendOptions.RADIUS
Deprecated.
Radius method allows corner creation with the specified radius value
|
static CornerTypeBuilder.BendOptions |
CornerTypeBuilder.BendOptions.RATIO_TO_DIAMETER
Deprecated.
Ratio to diameter method
|
Modifier and Type | Method and Description |
---|---|
CornerTypeBuilder.BendOptions |
CornerTypeBuilder.routeCornerBendOptions()
Deprecated.
Deprecated in NX8.5.0. Use
CornerTypeBuilder.routeCornerBendMethods() instead.
|
static CornerTypeBuilder.BendOptions |
CornerTypeBuilder.BendOptions.valueOf(int value)
Deprecated.
Returns the enum constant of the specified enum type with the specified value.
|
static CornerTypeBuilder.BendOptions |
CornerTypeBuilder.BendOptions.valueOf(String name)
Deprecated.
Returns the enum constant of the specified enum type with the specified name.
|
static CornerTypeBuilder.BendOptions[] |
CornerTypeBuilder.BendOptions.values()
Deprecated.
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CornerTypeBuilder.setRouteCornerBendOptions(CornerTypeBuilder.BendOptions routeCornerBendOptions)
Deprecated.
Deprecated in NX8.5.0. Use
CornerTypeBuilder.setRouteCornerBendMethods(nxopen.routing.CornerTypeBuilder.BendMethods) instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.