Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static AssignTangencyBuilder.TangencySide |
AssignTangencyBuilder.TangencySide.SOURCE
Assign tangency at source ControlPoint.
|
static AssignTangencyBuilder.TangencySide |
AssignTangencyBuilder.TangencySide.TARGET
Assign tangency at target ControlPoint.
|
static AssignTangencyBuilder.TangencySide |
AssignTangencyBuilder.TangencySide.UNDEFINED
The tangency side is undefined.
|
Modifier and Type | Method and Description |
---|---|
AssignTangencyBuilder.TangencySide |
AssignTangencyBuilder.assignTangencySide()
Returns the tangency side
AssignTangencyBuilder.TangencySide to assign tangency
License requirements: routing_base ("Routing Basic") Created in NX12.0.0 |
static AssignTangencyBuilder.TangencySide |
AssignTangencyBuilder.TangencySide.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AssignTangencyBuilder.TangencySide |
AssignTangencyBuilder.TangencySide.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AssignTangencyBuilder.TangencySide[] |
AssignTangencyBuilder.TangencySide.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AssignTangencyBuilder.assignTangency(Curve[] segments,
AssignTangencyBuilder.TangencySide tangencySide)
Assign tangency at specified side of the spline.
|
void |
AssignTangencyBuilder.assignTangencyAtPort(AssignTangencyBuilder.TangencySide tangencySide)
Assign tangency at attached port.
|
void |
AssignTangencyBuilder.removeTangency(AssignTangencyBuilder.TangencySide tangencySide)
Remove tangency at specified side of the spline.
|
void |
AssignTangencyBuilder.setAssignTangencySide(AssignTangencyBuilder.TangencySide tangencySide)
License requirements: routing_base ("Routing Basic") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.