Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static AlignStockBuilder.StockAlignmentMethod |
AlignStockBuilder.StockAlignmentMethod.ROUTING_OBJECT |
static AlignStockBuilder.StockAlignmentMethod |
AlignStockBuilder.StockAlignmentMethod.VECTOR_TO_VECTOR |
Modifier and Type | Method and Description |
---|---|
AlignStockBuilder.StockAlignmentMethod |
AlignStockBuilder.alignmentMethod()
Returns the alignment method.
|
static AlignStockBuilder.StockAlignmentMethod |
AlignStockBuilder.StockAlignmentMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AlignStockBuilder.StockAlignmentMethod |
AlignStockBuilder.StockAlignmentMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AlignStockBuilder.StockAlignmentMethod[] |
AlignStockBuilder.StockAlignmentMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AlignStockBuilder.setAlignmentMethod(AlignStockBuilder.StockAlignmentMethod alignmentMethod)
License requirements: routing_base ("Routing Basic") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.