public static class BranchPathNumberingBuilder.Sequence extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_LOWER_CASE
a, b, c, and so on
|
static int |
_NUMBERS
1, 2, 3, and so on
|
static int |
_UPPER_CASE
A, B, C, and so on
|
static BranchPathNumberingBuilder.Sequence |
LOWER_CASE
a, b, c, and so on
|
static BranchPathNumberingBuilder.Sequence |
NUMBERS
1, 2, 3, and so on
|
static BranchPathNumberingBuilder.Sequence |
UPPER_CASE
A, B, C, and so on
|
Modifier and Type | Method and Description |
---|---|
static BranchPathNumberingBuilder.Sequence |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BranchPathNumberingBuilder.Sequence |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BranchPathNumberingBuilder.Sequence[] |
values()
Returns an array that contains the values for this enum.
|
public static final BranchPathNumberingBuilder.Sequence NUMBERS
public static final BranchPathNumberingBuilder.Sequence UPPER_CASE
public static final BranchPathNumberingBuilder.Sequence LOWER_CASE
public static final int _NUMBERS
public static final int _UPPER_CASE
public static final int _LOWER_CASE
public static BranchPathNumberingBuilder.Sequence valueOf(int value)
public static BranchPathNumberingBuilder.Sequence valueOf(String name)
public static BranchPathNumberingBuilder.Sequence[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.