Package | Description |
---|---|
nxopen.presslinesimulation |
Provides classes and interfaces for Press Line Simulation.
|
Modifier and Type | Method and Description |
---|---|
UserMotionBuilder |
ApplicationManager.createUserMotionBuilder(Part part,
UserMotion userMotion)
Creates a
UserMotionBuilder
License requirements: nx_pls_die_checker (" NX Press Die Checker") Created in NX12.0.0 |
UserMotionBuilder |
UserMotionBuilderList.findItem(int index)
Returns the object at the input index.
|
UserMotionBuilder[] |
UserMotionBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
UserMotionBuilderList.append(UserMotionBuilder object)
Appends an object to the list
License requirements: None. |
void |
UserMotionBuilderList.append(UserMotionBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
UserMotionBuilderList.erase(UserMotionBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
UserMotionBuilderList.erase(UserMotionBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
UserMotionBuilderList.findIndex(UserMotionBuilder obj)
Finds the index where the input object appears.
|
void |
UserMotionBuilderList.insert(int location,
UserMotionBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
UserMotionBuilderList.setContents(UserMotionBuilder[] objects)
Sets the contents of the entire list.
|
void |
UserMotionBuilderList.swap(UserMotionBuilder object1,
UserMotionBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.