Package | Description |
---|---|
nxopen.presslinesimulation |
Provides classes and interfaces for Press Line Simulation.
|
Modifier and Type | Method and Description |
---|---|
MountPointBuilder |
MountPointBuilderList.findItem(int index)
Returns the object at the input index.
|
MountPointBuilder[] |
MountPointBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
MountPointBuilderList.append(MountPointBuilder object)
Appends an object to the list
License requirements: None. |
void |
MountPointBuilderList.append(MountPointBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
MountPointBuilderList.erase(MountPointBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
MountPointBuilderList.erase(MountPointBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
MountPointBuilderList.findIndex(MountPointBuilder obj)
Finds the index where the input object appears.
|
void |
MountPointBuilderList.insert(int location,
MountPointBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
MountPointBuilderList.setContents(MountPointBuilder[] objects)
Sets the contents of the entire list.
|
void |
MountPointBuilderList.swap(MountPointBuilder object1,
MountPointBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.