Package | Description |
---|---|
nxopen.presslinesimulation |
Provides classes and interfaces for Press Line Simulation.
|
Modifier and Type | Method and Description |
---|---|
MachineAdjustmentBuilder |
MachineAdjustmentBuilderList.findItem(int index)
Returns the object at the input index.
|
MachineAdjustmentBuilder[] |
MachineAdjustmentBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
MachineAdjustmentBuilderList.append(MachineAdjustmentBuilder object)
Appends an object to the list
License requirements: None. |
void |
MachineAdjustmentBuilderList.append(MachineAdjustmentBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
MachineAdjustmentBuilderList.erase(MachineAdjustmentBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
MachineAdjustmentBuilderList.erase(MachineAdjustmentBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
MachineAdjustmentBuilderList.findIndex(MachineAdjustmentBuilder obj)
Finds the index where the input object appears.
|
void |
MachineAdjustmentBuilderList.insert(int location,
MachineAdjustmentBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
MachineAdjustmentBuilderList.setContents(MachineAdjustmentBuilder[] objects)
Sets the contents of the entire list.
|
void |
MachineAdjustmentBuilderList.swap(MachineAdjustmentBuilder object1,
MachineAdjustmentBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.