Package | Description |
---|---|
nxopen.presslinesimulation |
Provides classes and interfaces for Press Line Simulation.
|
Modifier and Type | Method and Description |
---|---|
LinearCamBuilder |
ApplicationManager.createLinearCamBuilder(Part part,
LinearCam linearCam)
Creates a
LinearCamBuilder
License requirements: nx_pls_die_checker (" NX Press Die Checker") Created in NX12.0.0 |
LinearCamBuilder |
LinearCamBuilderList.findItem(int index)
Returns the object at the input index.
|
LinearCamBuilder[] |
LinearCamBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
LinearCamBuilderList.append(LinearCamBuilder object)
Appends an object to the list
License requirements: None. |
void |
LinearCamBuilderList.append(LinearCamBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
LinearCamBuilderList.erase(LinearCamBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
LinearCamBuilderList.erase(LinearCamBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
LinearCamBuilderList.findIndex(LinearCamBuilder obj)
Finds the index where the input object appears.
|
void |
LinearCamBuilderList.insert(int location,
LinearCamBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
LinearCamBuilderList.setContents(LinearCamBuilder[] objects)
Sets the contents of the entire list.
|
void |
LinearCamBuilderList.swap(LinearCamBuilder object1,
LinearCamBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.