Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static SessionVisualizationScreen.ViewTriadLocation |
SessionVisualizationScreen.ViewTriadLocation.BOTTOM_LEFT
Deprecated.
View triad display on the bottom left of the view
|
static SessionVisualizationScreen.ViewTriadLocation |
SessionVisualizationScreen.ViewTriadLocation.BOTTOM_RIGHT
Deprecated.
View triad display on the bottom right of the view
|
Modifier and Type | Method and Description |
---|---|
SessionVisualizationScreen.ViewTriadLocation |
SessionVisualizationScreen.triadLocation()
Deprecated.
Deprecated in NX12.0.0. Use
PartVisualizationScreen.triadLocation() and PartVisualizationScreen.setTriadLocation(nxopen.preferences.PartVisualizationScreen.ViewTriadLocation) instead
|
static SessionVisualizationScreen.ViewTriadLocation |
SessionVisualizationScreen.ViewTriadLocation.valueOf(int value)
Deprecated.
Returns the enum constant of the specified enum type with the specified value.
|
static SessionVisualizationScreen.ViewTriadLocation |
SessionVisualizationScreen.ViewTriadLocation.valueOf(String name)
Deprecated.
Returns the enum constant of the specified enum type with the specified name.
|
static SessionVisualizationScreen.ViewTriadLocation[] |
SessionVisualizationScreen.ViewTriadLocation.values()
Deprecated.
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SessionVisualizationScreen.setTriadLocation(SessionVisualizationScreen.ViewTriadLocation triadLocation)
Deprecated.
Deprecated in NX12.0.0. Use
PartVisualizationScreen.triadLocation() and PartVisualizationScreen.setTriadLocation(nxopen.preferences.PartVisualizationScreen.ViewTriadLocation) instead
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.