Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Method and Description |
---|---|
void |
ModelingViewHighQualityImage.plot(SessionVisualizationHighQualityImage.ResolutionType resolution,
int dotsPerInch,
SessionVisualizationHighQualityImage.PlotQualityType plotQuality,
String plotFileName)
Plots the previously generated high qualilty image of a view.
|
Modifier and Type | Field and Description |
---|---|
static SessionVisualizationHighQualityImage.ResolutionType |
SessionVisualizationHighQualityImage.ResolutionType.DRAFT |
static SessionVisualizationHighQualityImage.ResolutionType |
SessionVisualizationHighQualityImage.ResolutionType.HIGH |
static SessionVisualizationHighQualityImage.ResolutionType |
SessionVisualizationHighQualityImage.ResolutionType.LOW |
static SessionVisualizationHighQualityImage.ResolutionType |
SessionVisualizationHighQualityImage.ResolutionType.MEDIUM |
SessionVisualizationHighQualityImage.ResolutionType |
SessionVisualizationHighQualityImage.ResolutionData.resolution |
static SessionVisualizationHighQualityImage.ResolutionType |
SessionVisualizationHighQualityImage.ResolutionType.USER_DEFINED |
Modifier and Type | Method and Description |
---|---|
static SessionVisualizationHighQualityImage.ResolutionType |
SessionVisualizationHighQualityImage.ResolutionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionVisualizationHighQualityImage.ResolutionType |
SessionVisualizationHighQualityImage.ResolutionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionVisualizationHighQualityImage.ResolutionType[] |
SessionVisualizationHighQualityImage.ResolutionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SessionVisualizationHighQualityImage.setResolution(SessionVisualizationHighQualityImage.ResolutionType resolution,
int dotsPerInch)
Specifies the resolution to use when generating a High Quality Image.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.