Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static SessionSketch.BackgroundType |
SessionSketch.BackgroundType.INHERIT
Sketch background color is inherited from the parent application
|
static SessionSketch.BackgroundType |
SessionSketch.BackgroundType.PLAIN
Sketch background color is forced to the plain background color
|
Modifier and Type | Method and Description |
---|---|
SessionSketch.BackgroundType |
SessionSketch.backgroundOption()
Returns the background option
License requirements: None. |
static SessionSketch.BackgroundType |
SessionSketch.BackgroundType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionSketch.BackgroundType |
SessionSketch.BackgroundType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionSketch.BackgroundType[] |
SessionSketch.BackgroundType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SessionSketch.setBackgroundOption(SessionSketch.BackgroundType backgroundType)
Sets the background option
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.