Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static SessionModeling.SketchEditType |
SessionModeling.SketchEditType.DIRECT
Edit sketch without entering task environment
|
static SessionModeling.SketchEditType |
SessionModeling.SketchEditType.IN_TASK_ENVIRONMENT
Edit sketch in task environment
|
Modifier and Type | Method and Description |
---|---|
SessionModeling.SketchEditType |
SessionModeling.sketchEditOption()
Returns the option that determines whether or not task environment is used to edit the sketch
License requirements: None. |
static SessionModeling.SketchEditType |
SessionModeling.SketchEditType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionModeling.SketchEditType |
SessionModeling.SketchEditType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionModeling.SketchEditType[] |
SessionModeling.SketchEditType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SessionModeling.setSketchEditOption(SessionModeling.SketchEditType sketchEditOption)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.