Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static SessionModeling.SaveDataForFeatureEditOption |
SessionModeling.SaveDataForFeatureEditOption.FAST_ROLLBACK
Indicates the additional parasolid data is saved for faster rollback
|
static SessionModeling.SaveDataForFeatureEditOption |
SessionModeling.SaveDataForFeatureEditOption.FAST_ROLLBACK_AND_PREVIOUS_STATE_OF_FAILED_FEATURE
Indicates the additional parasolid data is saved for faster rollback and to show the previous state of failed feature
|
static SessionModeling.SaveDataForFeatureEditOption |
SessionModeling.SaveDataForFeatureEditOption.NONE
Indicates the no additional data is saved
|
Modifier and Type | Method and Description |
---|---|
SessionModeling.SaveDataForFeatureEditOption |
SessionModeling.saveDataForFeatureEdit()
Returns the option "Save Data for Feature Edit" specifies what additional data will
be saved in the part to enhance feature edit.
|
static SessionModeling.SaveDataForFeatureEditOption |
SessionModeling.SaveDataForFeatureEditOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionModeling.SaveDataForFeatureEditOption |
SessionModeling.SaveDataForFeatureEditOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionModeling.SaveDataForFeatureEditOption[] |
SessionModeling.SaveDataForFeatureEditOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SessionModeling.setSaveDataForFeatureEdit(SessionModeling.SaveDataForFeatureEditOption saveDataForFeatureEdit)
Sets the option "Save Data for Feature Edit" specifies what additional data will
be saved in the part to enhance feature edit.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.