Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static SessionModeling.DynamicUpdateType |
SessionModeling.DynamicUpdateType.CONTINUOUS
Indicates that Dynamic Update type is continuous
|
static SessionModeling.DynamicUpdateType |
SessionModeling.DynamicUpdateType.INCREMENTAL
Indicates that Dynamic Update type is incremental
|
static SessionModeling.DynamicUpdateType |
SessionModeling.DynamicUpdateType.NONE
Indicates that Dynamic Update type is not selected, this option is deprecated from NX12.0
|
Modifier and Type | Method and Description |
---|---|
SessionModeling.DynamicUpdateType |
SessionModeling.dynamicUpdate()
Returns the dynamic update.
|
static SessionModeling.DynamicUpdateType |
SessionModeling.DynamicUpdateType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionModeling.DynamicUpdateType |
SessionModeling.DynamicUpdateType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionModeling.DynamicUpdateType[] |
SessionModeling.DynamicUpdateType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SessionModeling.setDynamicUpdate(SessionModeling.DynamicUpdateType dynamicUpdate)
Sets the dynamic update.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.