Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static RoutingPath.RadiusUnits |
RoutingPath.RadiusUnits.INCHES
Use inch units
|
static RoutingPath.RadiusUnits |
RoutingPath.RadiusUnits.MILLIMETERS
Use metric (mm) units
|
static RoutingPath.RadiusUnits |
RoutingPath.RadiusUnits.NONE
Unspecified.
|
Modifier and Type | Method and Description |
---|---|
RoutingPath.RadiusUnits |
RoutingPath.getBendRadiusUnits()
Query bend radius units stored in path preferences
License requirements: routing_base ("Routing Basic") . |
static RoutingPath.RadiusUnits |
RoutingPath.RadiusUnits.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RoutingPath.RadiusUnits |
RoutingPath.RadiusUnits.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RoutingPath.RadiusUnits[] |
RoutingPath.RadiusUnits.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RoutingPath.setBendRadiusUnits(RoutingPath.RadiusUnits radiusUnits)
License requirements: routing_base ("Routing Basic") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.