Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static PartVisualizationScreen.ViewTriadLocation |
PartVisualizationScreen.ViewTriadLocation.BOTTOM_LEFT
View triad display on the bottom left of the view
|
static PartVisualizationScreen.ViewTriadLocation |
PartVisualizationScreen.ViewTriadLocation.BOTTOM_RIGHT
View triad display on the bottom right of the view
|
Modifier and Type | Method and Description |
---|---|
PartVisualizationScreen.ViewTriadLocation |
PartVisualizationScreen.triadLocation()
Returns the view triad location
License requirements: None. |
static PartVisualizationScreen.ViewTriadLocation |
PartVisualizationScreen.ViewTriadLocation.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartVisualizationScreen.ViewTriadLocation |
PartVisualizationScreen.ViewTriadLocation.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartVisualizationScreen.ViewTriadLocation[] |
PartVisualizationScreen.ViewTriadLocation.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PartVisualizationScreen.setTriadLocation(PartVisualizationScreen.ViewTriadLocation triadLocation)
Sets the view triad location
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.