Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static PartVisualizationEmphasis.SeeThruStyleType |
PartVisualizationEmphasis.SeeThruStyleType.LAYERS
Displays de-emphasized shaded geometry as translucent
layers with a single color.
|
static PartVisualizationEmphasis.SeeThruStyleType |
PartVisualizationEmphasis.SeeThruStyleType.ORIGINAL_COLOR_SHELL
Displays de-emphasized shaded geometry as a translucent
shell, preserving original colors.
|
static PartVisualizationEmphasis.SeeThruStyleType |
PartVisualizationEmphasis.SeeThruStyleType.SHELL
Displays de-emphasized shaded geometry as a translucent
shell with a single color.
|
Modifier and Type | Method and Description |
---|---|
PartVisualizationEmphasis.SeeThruStyleType |
PartVisualizationEmphasis.seeThruStyle()
Returns the See-Thru style that determines how translucency and color
are used to de-emphasize shaded geometry.
|
static PartVisualizationEmphasis.SeeThruStyleType |
PartVisualizationEmphasis.SeeThruStyleType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartVisualizationEmphasis.SeeThruStyleType |
PartVisualizationEmphasis.SeeThruStyleType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartVisualizationEmphasis.SeeThruStyleType[] |
PartVisualizationEmphasis.SeeThruStyleType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PartVisualizationEmphasis.setSeeThruStyle(PartVisualizationEmphasis.SeeThruStyleType seeThruStyle)
Sets the See-Thru style that determines how translucency and color
are used to de-emphasize shaded geometry.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.