Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Method and Description |
---|---|
IncludeModelCurvesOption |
ViewStyleHiddenLinesBuilder.includeModelCurvesOption()
Returns the include model curves option on the HIDDEN LINES tab of the View Style Dialog
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ViewStyleHiddenLinesBuilder.setIncludeModelCurvesOption(IncludeModelCurvesOption includeModelCurvesPointsOptionData)
License requirements: drafting ("DRAFTING") . |
Modifier and Type | Field and Description |
---|---|
static IncludeModelCurvesOption |
IncludeModelCurvesOption.NO
Do not process model curves for hidden line processing
|
static IncludeModelCurvesOption |
IncludeModelCurvesOption.YES
Process model curves for hidden line procesing
|
Modifier and Type | Method and Description |
---|---|
static IncludeModelCurvesOption |
IncludeModelCurvesOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static IncludeModelCurvesOption |
IncludeModelCurvesOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static IncludeModelCurvesOption[] |
IncludeModelCurvesOption.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.