public static class SessionModeling.FreeFormConstructionResultType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BSURFACE
Indicates the construction result option is B Surface
|
static int |
_PLANE
Indicates the construction result option is plane
|
static SessionModeling.FreeFormConstructionResultType |
BSURFACE
Indicates the construction result option is B Surface
|
static SessionModeling.FreeFormConstructionResultType |
PLANE
Indicates the construction result option is plane
|
Modifier and Type | Method and Description |
---|---|
static SessionModeling.FreeFormConstructionResultType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionModeling.FreeFormConstructionResultType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionModeling.FreeFormConstructionResultType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SessionModeling.FreeFormConstructionResultType PLANE
public static final SessionModeling.FreeFormConstructionResultType BSURFACE
public static final int _PLANE
public static final int _BSURFACE
public static SessionModeling.FreeFormConstructionResultType valueOf(int value)
public static SessionModeling.FreeFormConstructionResultType valueOf(String name)
public static SessionModeling.FreeFormConstructionResultType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.