public static class PartVisualizationEmphasis.WireframeBlendOptions extends Object implements Serializable
Modifier and Type | Field and Description |
---|---|
NXColor |
blendColor
the de-emphasis color that is blended with object colors
to de-emphasize wireframe geometry.
|
int |
blendPercentage
the percentage of the de-emphasis color that is blended
with object colors to de-emphasize wireframe geometry
It is a value between 10 and 100.
|
Constructor and Description |
---|
WireframeBlendOptions() |
WireframeBlendOptions(NXColor blendColorInitial,
int blendPercentageInitial)
Constructor for the WireframeBlendOptions object.
|
public NXColor blendColor
public int blendPercentage
public WireframeBlendOptions()
public WireframeBlendOptions(NXColor blendColorInitial, int blendPercentageInitial)
blendColorInitial
- the de-emphasis color that is blended with object colors
to de-emphasize wireframe geometry.blendPercentageInitial
- the percentage of the de-emphasis color that is blended
with object colors to de-emphasize wireframe geometry
It is a value between 10 and 100.Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.