Package | Description |
---|---|
nxopen.positioning |
Provides classes and interfaces for Assembly Positioning and Constraints.
|
Modifier and Type | Field and Description |
---|---|
static MatingConverter.PartContext |
MatingConverter.PartContext.IN_ALL_CHILDREN
Convert mating conditions in the owning part
and all children.
|
static MatingConverter.PartContext |
MatingConverter.PartContext.IN_LOADED_CHILDREN
Convert mating conditions in the owning part
and all loaded children.
|
static MatingConverter.PartContext |
MatingConverter.PartContext.IN_OWNING_PART
Convert mating conditions in the owning part
|
Modifier and Type | Method and Description |
---|---|
MatingConverter.PartContext |
MatingConverter.context()
Returns
the current conversion context in which mating conditions will be converted.
|
static MatingConverter.PartContext |
MatingConverter.PartContext.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MatingConverter.PartContext |
MatingConverter.PartContext.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MatingConverter.PartContext[] |
MatingConverter.PartContext.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MatingConverter.setContext(MatingConverter.PartContext context)
License requirements: assemblies ("ASSEMBLIES MODULE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.