public static class ComponentNetwork.ArrangementsMode extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EXISTING
Apply transforms in arrangements according to existing component properties.
|
static int |
_IN_USED
Apply transforms in the used arrangement only.
|
static ComponentNetwork.ArrangementsMode |
EXISTING
Apply transforms in arrangements according to existing component properties.
|
static ComponentNetwork.ArrangementsMode |
IN_USED
Apply transforms in the used arrangement only.
|
Modifier and Type | Method and Description |
---|---|
static ComponentNetwork.ArrangementsMode |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ComponentNetwork.ArrangementsMode |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ComponentNetwork.ArrangementsMode[] |
values()
Returns an array that contains the values for this enum.
|
public static final ComponentNetwork.ArrangementsMode EXISTING
public static final ComponentNetwork.ArrangementsMode IN_USED
public static final int _EXISTING
public static final int _IN_USED
public static ComponentNetwork.ArrangementsMode valueOf(int value)
public static ComponentNetwork.ArrangementsMode valueOf(String name)
public static ComponentNetwork.ArrangementsMode[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.