Package | Description |
---|---|
nxopen.pid |
Provides classes and interfaces for PID.
|
Modifier and Type | Field and Description |
---|---|
static ConnectionEndType |
ConnectionEndType.END
The end of connection.
|
static ConnectionEndType |
ConnectionEndType.START
The start of connection.
|
ConnectionEndType |
OffSheetConnectorBuilder.ConnectionData.type |
Modifier and Type | Method and Description |
---|---|
static ConnectionEndType |
ConnectionEndType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ConnectionEndType |
ConnectionEndType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ConnectionEndType[] |
ConnectionEndType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OffSheetConnectorBuilder.setConnection(ConnectionEndType type,
Pipe connection,
String connectionId)
To set the connection connecting to the OSC sheet element.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.