Package | Description |
---|---|
nxopen.pdm |
Provides classes and interfaces for PDM.
|
Modifier and Type | Field and Description |
---|---|
static PartOperationImportBuilder.ValidationRuleSetFileBrowseOption |
PartOperationImportBuilder.ValidationRuleSetFileBrowseOption.NATIVE |
static PartOperationImportBuilder.ValidationRuleSetFileBrowseOption |
PartOperationImportBuilder.ValidationRuleSetFileBrowseOption.TEAMCENTER |
Modifier and Type | Method and Description |
---|---|
PartOperationImportBuilder.ValidationRuleSetFileBrowseOption |
PartOperationValidationPropertiesBuilder.getValidationRuleSetBrowseOption()
Gets the validation rule set browse option
License requirements: None. |
PartOperationImportBuilder.ValidationRuleSetFileBrowseOption |
NativePartLogicalObject.getValidationRuleSetFileBrowseOption()
Gets the validation rule set file browse option defined for this part
License requirements: None. |
PartOperationImportBuilder.ValidationRuleSetFileBrowseOption |
PartOperationImportBuilder.validationRuleSetBrowseOption()
Returns the validation rule set browse option
License requirements: None. |
static PartOperationImportBuilder.ValidationRuleSetFileBrowseOption |
PartOperationImportBuilder.ValidationRuleSetFileBrowseOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartOperationImportBuilder.ValidationRuleSetFileBrowseOption |
PartOperationImportBuilder.ValidationRuleSetFileBrowseOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartOperationImportBuilder.ValidationRuleSetFileBrowseOption[] |
PartOperationImportBuilder.ValidationRuleSetFileBrowseOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PartOperationValidationPropertiesBuilder.setValidationRuleSetBrowseOption(PartOperationImportBuilder.ValidationRuleSetFileBrowseOption validationRuleSetBrowseOption)
Sets the validation rule set browse option
License requirements: assemblies ("ASSEMBLIES MODULE") . |
void |
PartOperationImportBuilder.setValidationRuleSetBrowseOption(PartOperationImportBuilder.ValidationRuleSetFileBrowseOption validationRuleSetBrowseOption)
License requirements: assemblies ("ASSEMBLIES MODULE") . |
void |
NativePartLogicalObject.setValidationRuleSetFileBrowseOption(PartOperationImportBuilder.ValidationRuleSetFileBrowseOption browseOption)
Sets the validation rule set file browse option defined for this part
License requirements: assemblies ("ASSEMBLIES MODULE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.