Package | Description |
---|---|
nxopen.pdm |
Provides classes and interfaces for PDM.
|
Modifier and Type | Field and Description |
---|---|
static PartOperationImportBuilder.Validation |
PartOperationImportBuilder.Validation.DEFAULT |
static PartOperationImportBuilder.Validation |
PartOperationImportBuilder.Validation.IMPORT_FROM_PART |
static PartOperationImportBuilder.Validation |
PartOperationImportBuilder.Validation.OFF |
static PartOperationImportBuilder.Validation |
PartOperationImportBuilder.Validation.RUN_VALIDATION |
static PartOperationImportBuilder.Validation |
PartOperationImportBuilder.Validation.RUN_VALIDATION_HYBRID |
Modifier and Type | Method and Description |
---|---|
PartOperationImportBuilder.Validation |
NativePartLogicalObject.getValidationMode()
Gets the validation mode setting defined for this part
License requirements: None. |
PartOperationImportBuilder.Validation |
PartOperationImportBuilder.validationMode()
Returns the validation mode
License requirements: None. |
static PartOperationImportBuilder.Validation |
PartOperationImportBuilder.Validation.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartOperationImportBuilder.Validation |
PartOperationImportBuilder.Validation.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartOperationImportBuilder.Validation[] |
PartOperationImportBuilder.Validation.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PartOperationImportBuilder.setValidationMode(PartOperationImportBuilder.Validation validationMode)
License requirements: assemblies ("ASSEMBLIES MODULE") . |
void |
NativePartLogicalObject.setValidationMode(PartOperationImportBuilder.Validation validationMode)
Sets the validation mode setting defined for this part
License requirements: assemblies ("ASSEMBLIES MODULE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.