Package | Description |
---|---|
nxopen.pdm |
Provides classes and interfaces for PDM.
|
Modifier and Type | Field and Description |
---|---|
static PartOperationImportBuilder.ConversionRule |
PartOperationImportBuilder.ConversionRule.AS_ID |
static PartOperationImportBuilder.ConversionRule |
PartOperationImportBuilder.ConversionRule.AS_IDAND_REVISION |
static PartOperationImportBuilder.ConversionRule |
PartOperationImportBuilder.ConversionRule.WITH_PREFIX |
static PartOperationImportBuilder.ConversionRule |
PartOperationImportBuilder.ConversionRule.WITH_REPLACE_STRING |
static PartOperationImportBuilder.ConversionRule |
PartOperationImportBuilder.ConversionRule.WITH_SUFFIX |
Modifier and Type | Method and Description |
---|---|
PartOperationImportBuilder.ConversionRule |
PartOperationImportBuilder.conversionType()
Returns the conversion type
License requirements: None. |
static PartOperationImportBuilder.ConversionRule |
PartOperationImportBuilder.ConversionRule.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartOperationImportBuilder.ConversionRule |
PartOperationImportBuilder.ConversionRule.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartOperationImportBuilder.ConversionRule[] |
PartOperationImportBuilder.ConversionRule.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PartOperationImportBuilder.setConversionType(PartOperationImportBuilder.ConversionRule conversionType)
License requirements: assemblies ("ASSEMBLIES MODULE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.