Modifier and Type | Interface and Description |
---|---|
static class |
PdmPart.CheckinInput
Reservation check-in input struct
|
static class |
PdmPart.CheckoutInput
Reservation check-out input struct
|
Modifier and Type | Method and Description |
---|---|
void |
assignPermanentName(String newFileName)
Assign a permanent name to the temporary part
License requirements: None. |
OperationErrors |
checkinParts(BasePart[] partsToCheckIn,
PdmPart.CheckinInput checkInInput)
Given an array of parts, check in the parts.
|
void |
checkout()
Checkout the part
License requirements: None. |
OperationErrors |
checkoutParts(BasePart[] partsToCheckOut,
PdmPart.CheckoutInput checkOutInput)
Given an array of parts, check out the parts.
|
AlternateIdManager |
newAlternateIdManager()
Create an instance of a
AlternateIdManager
class that will be used to create alternate ID information on the part. |
DatabaseAttributeManager |
newDatabaseAttributeManager()
Create an instance of a
DatabaseAttributeManager
class that will be used to modify database attributes of the part. |
void |
setDefaultFolderForPart()
Set default folder for the part in which it is to be saved
License requirements: None. |
void |
setPreciseStructureOnSave(BasePart[] partsToSetPreciseOnSave)
Given an array of parts, Parts to set precise structure on save.
|
AlternateIdManager newAlternateIdManager() throws NXException, RemoteException
AlternateIdManager
class that will be used to create alternate ID information on the part.
AlternateIdManager
instanceNXException
RemoteException
DatabaseAttributeManager newDatabaseAttributeManager() throws NXException, RemoteException
DatabaseAttributeManager
class that will be used to modify database attributes of the part.
DatabaseAttributeManager
instanceNXException
RemoteException
void checkout() throws NXException, RemoteException
NXException
RemoteException
void assignPermanentName(String newFileName) throws NXException, RemoteException
newFileName
- name of new part file to createNXException
RemoteException
void setDefaultFolderForPart() throws NXException, RemoteException
NXException
RemoteException
OperationErrors checkoutParts(BasePart[] partsToCheckOut, PdmPart.CheckoutInput checkOutInput) throws NXException, RemoteException
partsToCheckOut
- Array of parts to check outcheckOutInput
- Input which control the check out behaviorNXException
RemoteException
OperationErrors checkinParts(BasePart[] partsToCheckIn, PdmPart.CheckinInput checkInInput) throws NXException, RemoteException
partsToCheckIn
- Array of parts to check incheckInInput
- Input which control the check in behaviorNXException
RemoteException
void setPreciseStructureOnSave(BasePart[] partsToSetPreciseOnSave) throws NXException, RemoteException
partsToSetPreciseOnSave
- Array of parts to set precise structure on saveNXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.