public static class OptimizationBuilder.OptimizationTargetType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MAXIMUM
Target is maximum value of design objective
|
static int |
_MINIMUM
Target is minimum value of design objective
|
static int |
_TARGET
Target is specified value of design objective
|
static OptimizationBuilder.OptimizationTargetType |
MAXIMUM
Target is maximum value of design objective
|
static OptimizationBuilder.OptimizationTargetType |
MINIMUM
Target is minimum value of design objective
|
static OptimizationBuilder.OptimizationTargetType |
TARGET
Target is specified value of design objective
|
Modifier and Type | Method and Description |
---|---|
static OptimizationBuilder.OptimizationTargetType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OptimizationBuilder.OptimizationTargetType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OptimizationBuilder.OptimizationTargetType[] |
values()
Returns an array that contains the values for this enum.
|
public static final OptimizationBuilder.OptimizationTargetType MINIMUM
public static final OptimizationBuilder.OptimizationTargetType MAXIMUM
public static final OptimizationBuilder.OptimizationTargetType TARGET
public static final int _MINIMUM
public static final int _MAXIMUM
public static final int _TARGET
public static OptimizationBuilder.OptimizationTargetType valueOf(int value)
public static OptimizationBuilder.OptimizationTargetType valueOf(String name)
public static OptimizationBuilder.OptimizationTargetType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.