public static class TirePropertyCdBuilder.ModelType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CDT30 |
static int |
_CDT30HPS |
static int |
_CDT40 |
static int |
_CDT50 |
static TirePropertyCdBuilder.ModelType |
CDT30 |
static TirePropertyCdBuilder.ModelType |
CDT30HPS |
static TirePropertyCdBuilder.ModelType |
CDT40 |
static TirePropertyCdBuilder.ModelType |
CDT50 |
Modifier and Type | Method and Description |
---|---|
static TirePropertyCdBuilder.ModelType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TirePropertyCdBuilder.ModelType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TirePropertyCdBuilder.ModelType[] |
values()
Returns an array that contains the values for this enum.
|
public static final TirePropertyCdBuilder.ModelType CDT30
public static final TirePropertyCdBuilder.ModelType CDT30HPS
public static final TirePropertyCdBuilder.ModelType CDT40
public static final TirePropertyCdBuilder.ModelType CDT50
public static final int _CDT30
public static final int _CDT30HPS
public static final int _CDT40
public static final int _CDT50
public static TirePropertyCdBuilder.ModelType valueOf(int value)
public static TirePropertyCdBuilder.ModelType valueOf(String name)
public static TirePropertyCdBuilder.ModelType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.