public class ForceValueTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CONSTANT
constant type use constant value define force magnitude
|
static int |
_FUNCTION
function type use function define force magnitude
|
static int |
_PROFILE
profile type use profiles to define force magnitude
|
static ForceValueTypes |
CONSTANT
constant type use constant value define force magnitude
|
static ForceValueTypes |
FUNCTION
function type use function define force magnitude
|
static ForceValueTypes |
PROFILE
profile type use profiles to define force magnitude
|
Modifier and Type | Method and Description |
---|---|
static ForceValueTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ForceValueTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ForceValueTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final ForceValueTypes CONSTANT
public static final ForceValueTypes FUNCTION
public static final ForceValueTypes PROFILE
public static final int _CONSTANT
public static final int _FUNCTION
public static final int _PROFILE
public static ForceValueTypes valueOf(int value)
public static ForceValueTypes valueOf(String name)
public static ForceValueTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.